How do users assign cameras or monitors to a specific number in the WS5000 software?

Issue

How do users assign cameras or monitors to a specific number in the WS5000 software?

Product Line

Pelco Video Management

Environment

  • Endura WS5000- All versions
  • VCD5200
  • Decoder

Cause

The procedure to assign a camera or monitor a specific number is needed.

Resolution

Note: Only users with Administrator rights can access the Endura Workstation 'Setup' screen.
 
Assigning cameras to a specific number

  1. Access the Endura Workstation's 'Setup' screen, by either clicking on the Setup button in the toolbar or by pressing CTRL + Shift + S.
  2. Click on the Devices tab.
  3. Click on the camera to modify. Settings for that camera should now appear on the right side of the screen.
  4. Select the number from a drop down menu, next to 'Camera Number,' to assign to the camera (highlighted below in red).
  5. Click on the OK button to save the changes.



Assigning Monitors to a Specific Number
 

  1. Access the Endura Workstation's 'Setup' screen, by either clicking on the Setup button in the toolbar or by pressing CTRL + Shift + S.
  2. Click on the Devices tab.
  3. Click on the monitor to modify. Settings for that monitor should now appear on the right side of the screen.
  4. Select the number from a drop down menu, next to 'Monitor Number,' to assign to the monitor (highlighted below in red).
  5. Click on the OK button to save the changes.