How do users determine the Manager NSM within an NSM pool?

Issue

How do users determine the Manager NSM within an NSM pool?

Product Line

Pelco Video Management

Environment

Endura NSM5200- All versions

Cause

Need to determine which NSM in the pool is acting as manager.

Resolution

The current NSM5200 that is promoted as a Recording Pool Manager will be listed under the Model "NSM5200" within the Endura Utilities "System Attributes" tab, whereas the Pool Members will only be listed under the "NSD" Model (note: The manager will be in NSD as well).