How can users change the resolution of the JPEG image output on Sarix series cameras?

Issue

How can users change the resolution of the JPEG image output on Sarix series cameras?

Product Line

Pelco Cameras

Environment

Sarix cameras- All versions

Cause

Information regarding the resolution of the jpeg image output on Sarix model cameras is needed.

Resolution

Note: The number of streams and type of streams will vary by camera model. To view the streams available on a Sarix camera, please refer to Determining available streams on the Sarix IP camera entry for more details.

The URLs for accessing JPEGs are (Replace the IP address with the IP of the camera that you are working with.):

1920x1080 OR 1920x1080
http://10.220.196.186/jpeg?id=1 http://10.220.196.186/jpeg
640x352
http://10.220.196.186/jpeg?id=2