What is needed to mount an IP110 Camclosure onto a wall-like pendant?

Issue

What is needed to mount an IP110 Camclosure onto a wall-like pendant?

Product Line

Pelco Cameras

Environment

  • IP110 Camclosure series
  • IP111 Camclosure series

Cause

Wall mount the IP110/IP111 Camclosure Network Mini Dome Camera.

Resolution

An IP110-P pendant mount adapter and a SWM series compact wall mount with cable feedthrough is requires to mount an IP Camclosure onto a wall-like pendant.

NOTE: The IP110/IP111 Camclosure series and IP110-P are obsolete.