Endura workstation does not support the second video stream from Arecont cameras.

Issue

When using Arecont cameras and the workstation screen layout is 3X3 or higher, users will see a message that the camera cannot be displayed.

Product Line

Pelco Video Management

Environment

  • Endura Workstation
  • Arecont cameras

Cause

Using Arecont cameras with a workstation screen layout of 3X3 or higher.

Resolution

This is a compatibility issue between Arecont cameras and Endura workstation. To display video, the screen layout must be in single or quad mode.