How to adjust a Sarix camera's Digital Video Processing

Issue

How do users adjust a Sarix camera's digital processing?

Product Line

Pelco Cameras

Environment

Sarix

Cause

The camera's digital processing can be adjusted via the web interface.

Note: The following are minimum requirements for accessing the Sarix web application.  

  • Internet Explorer 7(or later)
  • Mozilla Firefox 3.0 (or later)
  • Quicktime

Note: The latest versions of Quicktime (certain version of 7.x and 10.0 for Mac OSX or 7.64 for Windows) contains a bug that prevents it from playing RTSP streams. 

Resolution

  1. Type the camera's IP address into a web browser.
  2. At the login prompt, enter the username and password.
    Username: admin
    Password: admin
  3. Once logged in, click on the Settings link in the top right.
  4. Click on the Imaging tab (near the top center of the screen).
  5. Configure the Sarix camera's digital processing settings. 

For more information regarding a Sarix camera's web application, please refer to IX Series Network Camera documentation.