Pole diameter for mounting the PA101

Issue

What is the minimum and maximum pole diameter for mounting the PA101?

Product Line

Pelco Cameras

Environment

  • PA101

Cause

Minimum and Maximum pole size to install PA101 pole adapter.

Resolution

Pole diameter specification:
 

Minimum 3 inches 7.62 centimeters
Maximum 8 inches 20.32 centimeters