What is the alarm response time from the alarm box to the CM6700/CM6800?

Issue

What is the alarm response time from the alarm box to the CM6700/CM6800?

Product Line

Pelco Matrix

Environment

CM6700 Matrix System all versions

CM6800 Matrix System all versions

ALM2064 all versions

Cause

Possible delay

Resolution

The CM6700/CM6800 response time from the point of contact closure on the alarm box to the appearance of video on the monitor is less than 150ms.