What is the Pin Out assignment for the Spectra Mini Interface cable?

Issue

  • What is the Pin Out assignment for the Spectra Mini Interface cable?
  • What color pinout for PTZ on the spectra Mini?

Product Line

Pelco Cameras

Environment

  • Spectra Mini analog series
  • SD4-W0
  • SD4-B0

Cause

Determine the function of the color wires and pin number on the interface cable.

Resolution

Please refer to the Pin Out chart below.

  • Cable is an RJ45 10pin connection with flying leads on opposite end.
  • Cable is 24" in length.
  •  Part Number for replacement cable is WA02-4654-005B
Pin
Color
Function
1
ORANGE
UTP-
2
WHITE/ORANGE
UTP+
3
GREEN
RX-
4
WHITE/GREEN
RX+
5
BLUE
TX-
6
WHITE/BLUE
TX+
7
NOT USED
---
8
NOT USED
---
9
BROWN
24 VAC
10
WHITE/BROWN
24 VAC