Why does the Spectra IV have no analog ptz control with the TXB-IP inserted?

Issue

Why does the Spectra IV have no analog ptz control with the TXB-IP inserted?

Product Line

Pelco Cameras

Environment

  • Spectra IV
  • TXB-IP

Cause

A network connection is required to establish analog ptz control.

Resolution

The Spectra IV with TXB-IP inserted does not support analog (two wire or coaxitron) control when there is no network connection established. Once a network connection is established it could take up to 10 minutes for control connection to begin.