How do I set the dip switch address on the CM6800 Matrix Switcher?

Issue

How do I set the dip switch address on the CM6800 Matrix Switcher?

Product Line

Pelco Matrix

Environment

  • CM6800 Matrix Switcher
  • KBD300A keyboard

Cause

Configure device address reside on the KBD300A and not on the CM6800 Switcher.

Resolution

There is no address setting for the dip switches on the CM6800, any address settings would be for the keyboards and are set on them.

They are set from the first 4 switches on the KBD300A. SW1-1 being the lowest bit.
 

ADDRESS SW1 SW2 SW3 SW4
0 OFF OFF OFF OFF
1 ON OFF OFF OFF
2 OFF ON OFF OFF
3 ON ON OFF OFF
4 OFF OFF ON OFF
5 ON OFF ON OFF
6 ON OFF ON OFF
7 ON ON ON OFF