How do I reset the Sarix ID series to factory default

Issue

What is the process to reset the ID Sarix IP indoor dome series?

Product Line

Pelco Cameras

Environment

Sarix ID Series Indoor Dome

  • ID10DN
  • IDE20DN

Cause

Camera will not pick up IP address from DHCP server and require defaulting camera settings.

Resolution

Remove the trim ring and underneath it is a hole marked "R". Use a paper clip to push in the hole gently and hold the button down for ten seconds. This will reset the camera.  The power LED turns red briefly, then blinks green while requesting a DHCP address.  When the IP address is assigned, the LED glows solid green.

Default IP is 192.168.0.20 thru 23

Make sure the PC is on the same Network  192.168.0.X