Do I need an adapter for the IE Sarix series to use a surface mount?

Issue

Do I need an adapter for the IE Sarix series to use a surface mount?

Product Line

Pelco Cameras

Environment

Sarix IE series- All versions

Cause

Information regarding the necessity of an adapter for the IE series to be used in a surface mount is needed.

Resolution

Yes. This is the part number for the surface mount, IE-S.