Can I use a different lens on the Sarix IX IP camera series?

Issue

Can I use a different lens on the Sarix IX IP camera series?

Product Line

Pelco Cameras

Environment

Sarix IX series- All versions

Cause

Information regarding the lenses for the Sarix IX series is needed.

Resolution

Depending on the model of the Sarix IX IP camera. IXS0 series use the varifocal lenses. There are 3 lens options:

  • 13VD2.5-6
  • 13VD2.8-12
  • 13VD5-50

The higher megapixel Sarix cameras IX10, IXE20, and IX30 use megapixel lenses. There are 4 mega pixel lens models:

  • 13M2.2-6
  • 13M2.8-8
  • 13M2.8-12
  • 13M15-50

Note: The use of standard definition lenses on higher megapixel Sarix models will limit the resolution of the camera, creating poor image quality.