How do I program the camera input to work with the Genex Multiplexer when connected to the CM6800E Matrix Switcher?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Connecting a Genex Multiplexer to the CM6800E Matrix Switcher?

Product Line

Pelco Matrix

Environment

Genex Multiplexer most versions

CM6800E Matrix Switcher all versions

Cause

Multi-screen display is required.

Resolution

  1. Enter the menu of the CM6800 Matrix Switcher
  2. Next select the camera tab
  3. Under control select multiplexer