How do I remove the CONFIGURATION DONE text from the video screen?

Issue

When using Spectra or Esprit, How do I remove the "CONFIGURATION DONE" text overlaid on the video screen?

Product Line

Pelco Cameras

Environment

  • Spectra IV SL/SE
  • Esprit Series
  • ExSite PTZ

Cause

The system performs a sequence configuration once powered on. When the configuration is done, the configuration setting is displayed on the monitor.

Resolution

The following is an example of what you might see when the system passed the sequence configuration. It displays the settings of the dome such as the dome version, addresses, and communication. The information will remain on the monitor until dome operation begins (PTZ control).

PelcoSpectra IV SL/Spectra IV SE
Version X.XX
D Address: 1
P Address: 2
Comm2400, N, 8, 1
CONFIGURE DONE