What are the available input/output connectors on the VCD5000?

Issue

What are the available input/output connectors on the VCD5000?

Product Line

Pelco Video Management

Environment

Endura VCD5000- All versions

Cause

Information regarding the available inputs and outputs on the VCD500 is needed.

Resolution



 

Video out
The VD5100 provides multiple video output options: up to three NTSC/PAL composite video outputs (BNC), up to three S-video outputs, and up to three VGA outputs.