Program a pattern with the CM6700 and the KBD300A.

Issue

How do I program a pattern with the CM6700 and the KBD300A?

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • CM6700 system
  • KBD300A keyboard
  • Spectra Series
  • Esprit Series
  • ExSite Series

Cause

Program a camera to run a continuous movement using KBD300A.

Resolution

  1. Select the camera you wish to program a pattern for.
  2. Press the pattern number then hold down the pattern button for 2 seconds, the monitor will indicate that the camera is in programming pattern mode.
  3. Move the camera around for the desired pattern.
  4. Press ACK  when you are finished, and the pattern will be programmed and stored in the camera.