How do I wire a CM9760 Matrix Switcher to CDU-T to Spectra cameras?

Issue

How do I wire a CM9760 Matrix Switcher to CDU-T to Spectra cameras?

Product Line

Pelco Matrix

Environment

CM9760-CDU-T

Cause

Where to connect wires on CM9760-CDU-T

Resolution

From the CC1 Sercom use a reversed cable, that is marked with a red band and each in labeled reversed. The from the back of the CDU-T you run a 2 wire to the Spectra camera, hooking to the RX+ and RX- keeping polarity the same. If you are daisy chaining from there hook the wires to the next camera also to RX + and - following the same pattern