Pole mount adapter for use with the WCS1-4

Issue

What pole mount adapter can be used with the WCS1-4?

Product Line

Pelco Transmission & Power

Environment

  • WCS1-4
  • PA402

Cause

Installation requires round pole mounting option for WCS1-4

Resolution

  • A pole mount adapter that may be used with the WCS1-4 is part number PA402.
  • The PA402 is provided with three stainless steel mounting straps.
  • Straps fit 3-inch (7.62 cm) to 8-inch (20.32 cm) diameter round pole.