How do I login locally at the DX8000/DX8100?

Issue

Need to login locally at the DX8000/DX8100.

Product Line

Pelco Video Management

Environment

DX8000 Series Video Recorder.
DX8100
Series Hybrid Video Recorder (HVR).

Cause

User Login is not visible unless you right click the desired server.

Resolution

You must have a valid username and password to log in to the DX8000/DX8100. The username and password are case sensitive.

To log in with a username other than Guest, follow the steps below:
  1. From the DX8000/DX8100 main menu, go to File > User Login. The User Login dialog box opens.
  2. Enter a valid username in the UserName field and a valid password in the Password field.
  3. Click "OK".

 

Related Topics:

Default login for the DX8000 Digital Video Recorder.

Default username and password for the DX8100 Series