Where can users modify brightness on Sarix web client?

Issue

Where can users modify brightness on Sarix web client?

Product Line

Pelco Cameras

Environment

Sarix cameras- All versions

Cause

Information regarding the brightness configuration of Sarix cameras is needed.

Resolution

  1. When viewing from the web client, log on and select Settings.
  2. A drop down menu bar on the top of the web client will appear. 
  3. Select the General from under the Imaging tab. 
  4. You can change the brightness level of the camera by adjusting the contrast or saturation.