What are the dome drives model numbers for the Spectra IV IP?

Issue

What are the dome drives model numbers for the Spectra IV IP?

Product Line

Pelco Cameras

Environment

  • SD4N36 Models
  • SD4N29 Models
  • SD4N23 Models

Cause

Dome Drive camera model for replacement.

Resolution

The Spectra IV IP consists of four components. The Back Box (housing), The Dome Drive (camera), Lower Dome (bubble and trim ring) and TXB-IP-P or TXB-IP-F encoder card. The following list is of the camera module only.

The model numbers are DD423, DD427, DD4CBW35. See below for camera specification.