How many CM9700-SER's or Sercom Cards can I add to the Cm9700-CC1?

Issue

How many CM9700-SER's or Sercom Cards can I add to the Cm9700-CC1?

Product Line

Pelco Matrix

Environment

CM700-CC1

CM9700 Matrix Switcher

Cause

Additional Sercomm port

Resolution

You can put a maximum of 4 Sercom cards/ 32�RJ-45 Ports�.