Issue
How many Volt-Amps (VA) does it take for the Spectra IV IP Outdoor model?
Product Line
Pelco Cameras
Environment
Spectra IV IP series
Cause
The measurement of power to operate the Spectra IV IP Outdoor.
Resolution
Input Power
- 24 VAC 23 VA nominal (without heater); 73 VA nominal (with heater)
- 24 VDC 0.7 A nominal (without heater); 3 A nominal (with heater)
- Fuse 1.25 A