Where can I find the MAC address for the Spectra IV?

Issue

Where can I find the MAC address for the Spectra IV?

Product Line

Pelco Cameras

Environment

  • SD4E Models
  • SD4N Models
  • TXB-IP-P or TXB-IP-F
  • TXB-N-P or TXB-IP-F

Cause

MAC address location

Resolution

There is no MAC address for the Spectra IV it is not ethernet device. If it has a TXB-N or TXB-IP installed, the IP address and MAC address show up in the device utility when the camera is called up.