Does the outdoor Camclosure model PA01-0045-00A0G come with components?

Issue

Does the outdoor Camclosure model PA01-0045-00A0G come with components?

Product Line

Pelco Cameras

Environment

Outdoor Camclosure (model: PA01-0045-00A0G)

Cause

Verify components received with build of materials (BOM)

Resolution

Yes. The Outdoor Camclosure model PA01-0045-00A0G come with the following:

  • Cap part number CP06-0151-1107
  • A diode part number DO11-1500-4005
  • PC board 24VDC fan rectifier part number PC01-0045-00A0, one of each