Does the Sarix IM mini dome series have window blanking?

Issue

Does the Sarix IM mini dome series have window blanking?

Product Line

Pelco Cameras

Environment

Sarix IM series- All versions

Cause

Information regarding window blanking on the IM series of Sarix cameras is needed.

Need to block a specific area from being recorded.

Resolution

The Sarix IM mini dome supports up to four different blanked areas. This feature is listed under Imaging settings in the web interface for the camera.

 

 

To configure Window Blanking on a Sarix IM Series:

  1. Connect to the Sarix camera via IE.
     
  2. Login to the camera.
     
  3. Go to settings.
     
  4. Take the mouse pointer to Imaging and select Window Blanking.
     
  5. Turn Window Blanking On.
     
  6. Configure window blanking as needed.

    Note: IMP521 supports up to seven window blanking /privacy areas.