What IP TXB card is used for Spectra IV?

Issue

How do I convert an analog Spectra IV to a network camera?

Product Line

Pelco Cameras

Environment

  • Spectra IV v1.07 or higher
  • IP TXB Translator Board
    • TXB-IP-F
    • TXB-IP-P
    • TXB-N-F
    • TXB-N-P

Cause

Conversion of Spectra IV analog to IP camera.

Resolution

The SD4E (H.264, MPEG-4,MJPEG) Series features the following IP card:
TXB-N-F       For flush in-ceiling model.
TXB-N-P       For pendant model.

The SD4N  (MPEG-4) Series features the following IP card:
TXB-IP-F      For flush in-ceiling model.
TXB-IP-P        For pendant model.

Note: TXB encoder's RJ-45 pig tail part number: WA01-6104-001A