What happens if multiple users try to control PTZ at once in Endura?

Issue

What happens if multiple users try to control PTZ at once in Endura?

Product Line

Pelco Video Management

Environment

Endura WS5000- All versions

Cause

Information regarding the outcome if multiple users try to PTZ the same camera simultaneously is needed.

Resolution

The user with the highest device priority level will have control of PTZ. If both users are have the same priority, it will be based on first come first serve.