Is there a pressurized Spectra IV in an IP version available?

Issue

Is there a pressurized Spectra IV in an IP version available?

Product Line

Pelco Cameras

Environment

  • SD4E Series
  • SMR#1-1WDCRV with TXB-N-F ( H.264 )
  • SMR#1-IDT4X with TXB-IP-F  ( MJPEG )X


    (

Cause

Spectra IP with pressurized housing

Resolution

You can get a Pressurized Spectra IV camera as an IP based camera by ordering the model you want under the SMR of 1-1WDCRV with the addition of the TXB-N-F module.


The following are model numbers for ANALOG Spectra IV models.

1. Select Analog Spectrra IV model from the following chart:.
2. Select desired SMR (that will include the TXB encoder) from the Environment section.
3. Place order for Analog Spectra with reference to SMR#.