How do I set the audio to the internal microphone on the Sarix IM mini-dome series?

Issue

How do I set the audio to the internal microphone on the Sarix IM mini-dome series?

Product Line

Pelco Cameras

Environment

Sarix IM series- All versions

Cause

Information on how to set the audio to the internal microphone for the Sarix IM cameras is needed.

Resolution

Go into the audio configuration setting and set the audio to enabled. The best settings in most situations are;

  1. Native microphone line in.
  2. 8KHZ
  3. PMCU

Refer to page 46 in the IM Series Installation/Operation manual for information on audio configuration.

Checkmark Audio Enable for Microphone In.