How do I access the UDI5000 interface from the Endura Workstation?

Issue

How do I access the UDI5000 interface from the Endura Workstation?

Product Line

Pelco Video Management

Environment

  • Endura UDI5000-MTRX- All versions
  • Endura UDI5000-CAM- All versions

Cause

Information on how to access the web interface for a UDI5000 is needed.

Resolution

The UDI5000 is accessed via an internet browser, so just open a browser and type in the IP address. Endura Utilities will also start a web browser for you by selecting the Open Web Interface option in the right click menu.