What is the power consumption of RK5200PS-5U chassis?

Issue

What is the power consumption of RK5200PS-5U chassis?

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

Endura RK5200PS-5U

Cause

Information regarding power consumption is needed.

Resolution

ELECTRICAL
Input Voltage:                100 to 240 VAC, 50 to 60 Hz, autoranging, 3.6 A
Output Voltage:            12 VDC

Power Consumption:   Operating Maximum (noninclusive of components within the rack)

  • 100 VAC 75W, 256 BTU/H
  • 115 VAC 75W, 256 BTU/H
  • 220 VAC 70W, 239 BTU/H

NOTE:  BTU/H is based on 20% internal inefficiency rating; 80% of power output is consumed by NET5301 or NET5400T units.