What cameras are supported with the AUD-1 (audio dongle)

Issue

What cameras can I use with the Aud-1 (audio dongle)?

Product Line

Pelco Cameras, Pelco Video Management

Environment

Using a Sarix based camera with an external audio dongle

Cause

To determine which cameras will work with the AUD-1 audio dongle

Resolution

Any sarix camera that has a USB port and does not have an internal audio microphone or is wired for audio line in and line out can use the AUD-1.

 

See AUD-1 Installation Manual for more information.