What is the Ethernet connection type on the SM5000/SM5200?

Issue

What is the Ethernet connection type on the SM5000/SM5200?

Product Line

Pelco Video Management

Environment

Endura SM5000/SM5200- All versions

Cause

Information regarding the ethernet connection on an SM5000/SM5200 is needed.

Resolution

The System Manager needs to be on a 1GB network connection.