What are the available video compression formats in the Spectra IV IP?

Issue

What are the available video compression formats in the Spectra IV IP?

Product Line

Pelco Cameras

Environment

Spectra IV IP series

Cause

Depend on the installed Spectra IV IP system, it can be configured to the available encode format to save hard drive spaces and image quality. 

Resolution

Model Encoding Format
Spectra IV TXB-IP MPEG4, MJPEG
Spectra IV (Sarix Base) TXB-N H.264, MPEG4, MJPEG