What is the maximum number of camera inputs for the CM9765 Matrix Switcher/Controller?

Issue

What is the maximum number of camera inputs for the CM9765 Matrix Switcher/Controller?

Product Line

Pelco Matrix

Environment

  • CM9760
  • CM9760-MXB
  • CM9760-VCC

Cause

Maximum Camera Input for CM9760

Resolution


Microprocessor-Based Switcher/Controller, 2,048 Inputs, 512 Outputs
The 9765 System is a full-featured video matrix switching control system that allows users to view and control up to 2,048 cameras and 512 monitors on a single node. Up to 96 individual user-defined ID numbers can be assigned to allow or deny access to system functions.

Features:

  • Microprocessor-Based, Full Cross-Point Video Matrix 
  • High-Density Architecture Supports up to 256 Cameras and 16 Monitors in Each Bay
  • Control up to 2,048 Cameras and 512 Monitors in a Single Node or Expand Camera Capacity with a Multi-Node System (up to 24 Nodes