Where can users find possible, valid configuration settings for a particular cameras?

Issue

Where can users find possible, valid configuration settings for a particular cameras?

Product Line

Pelco Cameras

Environment

Sarix Series Cameras

Cause

Valid configuration settings

Resolution

One of the main features of Sarix's StreamConfiguration service (and any future product supporting this service) is that it will list all possible settings including possible valid values for these settings. This will also take into account possible values for one setting in relation to other settings that are interdependent. For example if the resolution and framerate settings are set above a certain threshold, then the sign setting will only allow a false value.

Although Pelco provides specification sheets, using the StreamConfiguration service is the only way to guarantee that you are receiving the most up to date information regarding camera configuration (for Pelco product lines such as Sarix).