What are recommended lenses for the IP3701?

Issue

What are recommended lenses for the IP3701?

Product Line

Pelco Cameras

Environment

IP3701

Cause

Recommended lenses

Resolution

Below are the available lenses including their focal lengths and description.

Note: This is based upon current availability and is subject to change. 

Model Description
13VA1-3 Manual Lens
13VA 2.8-12 Manual Lens
13VA3-8 Manual Lens
13VA5-40 Manual Lens
13VA5-50 Manual Lens
13VD1-3 Auto Iris Lens
13VD2.5-6 Auto Iris Lens
13VD2.8-12 Auto Iris Lens
13VD3-8 Auto Iris Lens
13VD5-40 Auto Iris Lens
13VD5-50 Auto Iris Lens
13VD5.5-82.5 Auto Iris Lens
13ZD6X8 Auto Iris, Zoom Lens
13ZD6X10 Auto Iris, Zoom Lens
13ZD6X15 Auto Iris, Zoom Lens
13ZD6X20 Auto Iris, Zoom Lens
13ZD5.5X30 Auto Iris, Zoom Lens