What is a Preset?

Issue

What is a Preset?

Product Line

Pelco Cameras

Environment

PTZ (Pan Tilt Zoom) cameras

Cause

Information about the function of the Preset feature.

Resolution

Preset - A preset is a script that allows users to a save a camera's position, zoom, and other settings such as auto-iris and auto-focus; collectively as a 'bookmark'. Users can save multiple presets per camera. For example if a user monitoring several specific points using the same camera, the user can set one preset for the main entrance with a moderate zoom value, and the user can set another preset for a vulnerable window, lying some ways from the main entrance, with a higher value zoom value and a specific position.