If I install the IX Sarix IP cameras series in the outdoor housing with a heater and blower, do I use power over ethernet (PoE)?

Issue

If I install the IX Sarix IP cameras series in the outdoor housing with a heater and blower, do I use power over ethernet (PoE)?

Product Line

Pelco Cameras

Environment

Sarix IX series- All versions

Cause

Information regarding the usage of POE is needed.

Resolution

No. Use 24 VAC and it will power everything, the heater, blower and camera.