In Digital Sentry RealVue Xpress, how do I check to see if the recording mode is on motion or timelapse?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

In Digital Sentry RealVue Xpress, how do I check to see if the recording mode is on motion or timelapse?

Product Line

Pelco Video Management

Environment

DigitalSentry RealVue Xpress version 7.1.47

Cause

When time-lapse and motion storage are scheduled, motion storage schedule and recording rate override the time-lapse recording schedule when a motion event occurred.

Resolution

To verify whether or not the Digital Sentry systems are in certain recording modes, please refer to page 28 and 29 for storage modes in the following manual:

Digital Sentry Software Operation/Installation Manual