How do I identify the total number physical NSM5200 units on the Endura network?

Issue

How do I identify the total number physical NSM5200 units on the Endura network?

Product Line

Pelco Video Management

Environment

Endura NSM5200- All versions

Endura Utilities - All versions

Cause

Information on how to determine the physical number of NSMs on the Endura network.

Resolution

The best way to identify the total number of physical NSM5200 units on the Endura network is to use the Endura Utilities.  With the Endura Utilities, search for all devices on the Endura network and located the model, "NSD" in the left hand column.  Reference the NSD to the device count.  The device count is the total number of physical NSM5200 units on the Endura Network.