Is an imagepak available for ID Sarix IP Indoor Domes?

Issue

Is an imagepak available for ID Sarix IP Indoor Domes?

Product Line

Pelco Cameras

Environment

Sarix ID series- All versions

Cause

Information regarding the availability of an imagepak for the ID series cameras is needed.

Resolution

If it is a megapixel camera the only available lens package is the 2.8.to 8 mm. The Standard definition cameras come in 3-8 mm, 2.8-12 mm package.