Does the auto tracking feature on a Spectra HD camera follow a person?

Issue

Does the auto tracking feature on a Spectra HD camera follow a person?

Product Line

Pelco Cameras

Environment

  • Spectra HD IP cameras
    • D5118
    • D5220
    • D5230

Cause

Supporting features

Resolution

The AutoTracker behavior detects and tracks movement in the camera's field of view. When the AutoTracker behavior is configured, the system automatically pans and tilts to follow the moving object until the object stops or disappears from the monitored area.

(Zone Settings) Optimize Zoom Settings for Objects of this Type: Defines the type of object to be tracked. Settings include person, car, car or person, and custom.