Firefighters Smoke Control Station Interface (FSCSI) database should consist entirely of internal points and point extensions

Issue

Why is it recommended that the Firefighters Smoke Control Station Interface (FSCSI) database consists entirely of internal points and point extensions?

Product Line

TAC I/NET

Environment

Firefighters Smoke Control Station Interface (FSCSI)

Cause

This allows the same database to be used regardless of whether the FSCSI is an ICI PCU or even an MRI.

Resolution

This allows the same database to be used regardless of whether the FSCSI is an ICI PCU or even an MRI. For more information see TCON 231, Smoke Control Systems Manual, Database Logic.