Using the DVR5100 Remote Client, how do I access the camera's configuration menu?

Issue

Using the DVR5100 Remote Client, how do I access the camera's configuration menu?

Product Line

Pelco Video Management

Environment

DVR5100 series hybrid video recorder (HVRs)

Cause

Configure camera settings using DVR5100 remote client

Resolution

To access the camera's configuration menu do the following:

  1. Log in using a user account with administrative permissions.
  2. Select desired camera in the cameras list and drag it to the workspace.
  3. Right click on the video for that camera and select "Enter Menu" to bring up the camera's OSD(On Screen Display).
  4. To clear the camera's OSD when finished, right click and select "Exit Menu"