Differentiate monitors connected to the Endura VCD5202 Video Console Display and NET5402R-HD Decoder.

Issue

In a monitor wall, how do I differentiate monitors connected to the Endura VCD5202 Video Console Display and NET5402R-HD Decoder?

Product Line

Pelco Video Management

Environment

  • Endura VCD5202- All versions
  • Endura NET5402R- All versions

Cause

It is necessary to determine which device is connected to a specific monitor.

Resolution

One simple solution is to change the border color on the monitors. Using the WS5000 Endura Advanced Management Software, follow the following procedure to modify the border color. 

1) Go to the Setup page
2) Under Devices tab,  click Filters
3) Click on Device Type
4) Click Monitor
5) Select device monitor to modify (Under "Devices" on left pane.)
6) Next to "Border" click Modify to change the color