What is the maximum number of camera inputs for the CM6700 Matrix Switcher/Controller?

Issue

What is the maximum number of camera inputs for the CM6700 Matrix Switcher/Controller?

Product Line

Pelco Matrix

Environment

  • CM6700-MXB2
  • CM6700-MXB4

Cause

Maximum Camera Inputs

Resolution

The CM6700 Matrix switcher/controller is a very affordable, highly versatile, full-featured cross-point matrix switcher. The CM6700 provides switching and control for 16 video inputs and up to 4 monitor outputs from any one of up to 8 keyboards.